uEye XC Industrial camera as webcam

IDS industrial camera uEye XC in front of a grey background.

Automatically perfect images

Connect the camera, focus automatically, get a perfectly sharp image or video - this is especially useful when object distances change frequently. Webcams are therefore used in many kiosk and robotics applications. However, they are usually designed for the consumer market. The uEye XC is different: it closes the market gap between industrial camera and webcam. Depending on preference, customers can choose between variants with USB3 Vision (programmable) and UVC protocol (plug&play) for the autofocus camera. From kiosk systems to logistics and robotics - the uEye XC shows what counts.

USB3

UVC

Auto-image control

Autofocus

Plug & Play

Compact dimensions

13 megapixel

Ready-to-use camera

Just plug in and get started

The uEye XC is an industrial camera with the simplicity of a webcam. Setting up and operating the camera only requires a cable connection. After that, the autofocus camera with the 13 MP onsemi sensor AR1335 immediately delivers high-resolution, detailed images and videos. With the quickly exchangeable macro lens, you can easily shorten the minimum object distance of the camera. This makes it suitable for close-up applications, for example in medical technology.

Many front and rear parts of the IDS uEye XC camera housing.

Long product life cycle

Use of industrial components

Unlike consumer webcams, the uEye XC camera is designed for industrial use. Its components score with long availability - a must for industrial applications. Useful features such as digital zoom, auto white balance and colour correction ensure that you can capture all details perfectly. If required, you can program the USB3 Vision industrial camera specifically for your application with IDS peak, the powerful software development kit from IDS. If you choose a model with UVC protocol (USB Video Class), you will benefit from the typical webcam "plug&play" without the need for additional drivers.

Eine Hand hält die IDS Industriekamera uEye XC.

Compact lightweight

Highly versatile autofocus camera

The uEye XC is characterised by its particularly elegant and lightweight magnesium housing. With dimensions of only 32 x 61 x 19 mm (W x H x D), it is compact, sturdy despite its light weight and absolutely suitable for industrial use. Its 13 MP onsemi sensor delivers 20 fps at full resolution and, thanks to BSI technology, can easily handle changing light conditions. Available with USB3 and UVC (USB Video Class) as well as in a convenient starter set with accessories.

Glass bottles on a shelf containing orange liquid.

Quality control

For industrial production, the highest standards of quality and safety have to be met. The uEye XC shows its strengths in process and quality assurance, for example. This guarantees standardised, consistent quality of goods, improves the entire process and increases productivity.

One person is holding a flight ticket and a passport.

Kiosk systems

Whether cash, passport photo or postcard machines: uEye XC can be used in all kiosk systems. It makes customised service in photo-assisted terminals easy. In airports, combining uEye XC with passport readers is an ideal building block for property protection.

A robot arm places a cardboard box on a self-propelled robot.

Logistics automation

uEye XC helps to capture objects on conveyor belts, barcodes on parcels or labels on luggage. The autofocus camera provides a cost-effective solution to monitor, analyse and optimise operations from the first step to the last.

Computer in the laboratory, operated by a person wearing a blue glove.

Medical technology

In dermatology, the compact autofocus camera can be used to precisely detect the finest skin lesions using the macro lens. No matter if you are performing an online consultation or diagnosis: uEye XC guarantees high-quality images and is flexible in its handling.

Image by IDS technical author Heiko Seitz

Discover what uEye XC makes possible

An enlarged field on a euro banknote shows the zoom power of the uEye XC.

So much to discover: The autofocus camera automatically focuses on the intended subject and thus ensures a perfect distance setting. Here, the example shows the inside of a window (4 cm away from the camera), the outside of a window (8 cm), a cup placed on a facade projection (20 cm) and the surroundings (infinity). If necessary, the focus can also be controlled by software.

What customers say about uEye XC industrial cameras:

“The uEye XC fits perfectly with our system philosophy: It automatically delivers images without our users having to struggle with optical parameters.”

— David Fehrenbach, founder of preML —